i.MX6Q - GPIO Output and Blinking LED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q - GPIO Output and Blinking LED

ソリューションへジャンプ
2,926件の閲覧回数
yoshitakatakebe
Contributor II


Hi.

I'm working on MCIMX6-SDB (SABRE-SD).

SABRE-SD will be used to notify signal to another CPU Board by setting "GPIO_2" high/low.

In DESIGN_FILE (SPF-27392_C5.pdf), GPIO_2 is connected to "KEY_ROW6" signal and that connect to "USR_DEF_RED_LED". That makes D3 LED up/down.

So, I think that if GPIO_2 is set to high or low,  D3 LED blinks. Is it right?

If it is right, I have next question.

To blink D3 LED, GPIO1 bit2 is written 1 and 0, but D3 LED does not blink.

Registers were initialized as below, please tell me if there are some lack or trouble.

(1) Write 0x00000015 to IOMUXC_SW_MUX_CTL_PAD_GPIO02 (0x020E_0234).

(2) Write 0x0001b0b0 to IOMUXC_SW_PAD_CTL_PAD_GPIO02 (0x020E_0604)

(3) Write 0x00000004 to GPIO1_GDIR (0x0209_C004)

(iterate below)

(4) Write 0x00000004 to GPIO1_DR (0x0209_C000)

(5) Write 0x00000000 to GPIO1_DR (0x0209_C000)

ラベル(1)
0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yoshitaka

pelase refer to attached example for

toggling LED (D3, GPIO1_2) on i.MX6 SD-SDP board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yoshitaka

pelase refer to attached example for

toggling LED (D3, GPIO1_2) on i.MX6 SD-SDP board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,267件の閲覧回数
yoshitakatakebe
Contributor II

Hi Mr.igorpadykov.

It worked.

Thank you for your help.

Best regards

Yoshitaka

0 件の賞賛
返信