i.MX6DQ audio interface.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ audio interface.

ソリューションへジャンプ
1,708件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ audio interface.
Actually, our customer have used 3 audio inputs/outputs with SSI1 to SSI3.
In this case, can they add a new audio input/output with ESAI?

Would you let me know what is the maximum number of audio interface (SSI + ESAI) i.MX6DQ can be used?


Best Regards,
Satoshi Shimoda

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
1,565件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,566件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信