i.MX6DQ audio interface.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ audio interface.

Jump to solution
1,200 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ audio interface.
Actually, our customer have used 3 audio inputs/outputs with SSI1 to SSI3.
In this case, can they add a new audio input/output with ESAI?

Would you let me know what is the maximum number of audio interface (SSI + ESAI) i.MX6DQ can be used?


Best Regards,
Satoshi Shimoda

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
1,057 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,058 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply