i.MX6DQ IPU IC combining performance.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DQ IPU IC combining performance.

跳至解决方案
1,282 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL IPU CSI.

Please see the slide No. 56 of attached file in A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

It says the combining in the Image Conveter is upt to 40M pixels/sec with i.MX6DQ.

Next, please see chapter 37.1.2.1.5.3 in IMX6DQRM Rev.3, it says the IC perfomance is 200M pixels/sec for input and 100M pixels/sec for output.

To understand combining performance by Image Converter, which performance should I use?

Best Regards,

Satoshi Shimoda

标记 (4)
0 项奖励
回复
1 解答
1,154 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,155 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复