Hi community,
I have a question about i.MX6SDL IPU CSI.
Please see the slide No. 56 of attached file in A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
It says the combining in the Image Conveter is upt to 40M pixels/sec with i.MX6DQ.
Next, please see chapter 37.1.2.1.5.3 in IMX6DQRM Rev.3, it says the IC perfomance is 200M pixels/sec for input and 100M pixels/sec for output.
To understand combining performance by Image Converter, which performance should I use?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
Image Conveter suppots many operations and RM gives max. IC perfomance.
IC combining performance is given in presentation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
Image Conveter suppots many operations and RM gives max. IC perfomance.
IC combining performance is given in presentation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------