i.MX6DQ CSI performance.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ CSI performance.

Jump to solution
791 Views
keitanagashima
Senior Contributor I

Hi.

I'd like to know the CSI performance.

Is it possible to input dual 1080p@60 video into CSI?

I think it is impossible.

Because, there is below limitation.

F = FH * FW * FPS * BI * DF

Where

   FH = frame height (in pixels)

   FW = Frame width (in pixels)

   fps = frame rate (frames per second) ? BI = typically 35% overhead, should be assumed as 1.35. The actual blanking intervals are a parameter of the attached device.

   DF = data format, defines the number of cycles needed to send a single pixel.

If one use a 1080p@60 camera;

167.96MHz = 1080 * 1920 * 60 * 1.35 * 1 < 240MHz --> OK

In case of Dual camera;

335.92MHz = 1080 * 1920 * 60 * 1.35 * 1 * 2 > 240MHz --> NG


If one use a 1080p@60 and a 720p@60 camera;

242.6MHz = (1080 * 1920 * 60 * 1.35 * 1) + (1280 * 720 *60 *1.35 * 1) > 240MHz --> NG


Is my understanding right?


Keita


Labels (3)
0 Kudos
1 Solution
571 Views
Yuri
NXP Employee
NXP Employee

Correct for single IPU.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
572 Views
Yuri
NXP Employee
NXP Employee

Correct for single IPU.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
571 Views
keitanagashima
Senior Contributor I

Dear Yuri,

Hello.

Thank you for your reply.


>Correct for single IPU.

If one use i.MX6DQ (= 2 IPUs), is it possible to input dual 1080p@60 video?

IPU0 <-- YUV422 1080p@60

IPU1 <-- YUV422 1080p@60

Keita

0 Kudos
571 Views
Yuri
NXP Employee
NXP Employee

Yes.

0 Kudos