UART TxD/RxD in DCE mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART TxD/RxD in DCE mode

跳至解决方案
1,884 次查看
keitanagashima
Senior Contributor I

Hi.

Refer to 64.2.1.1 Serial/IrDA Signals IMX6SDLRM_Rev.1.

There is description of I/O direction each mode (DCE/DTE).

When I set DCE mode, TxD and RxD became opposite I/O direction.

Is it right operation?

Keita

标签 (3)
0 项奖励
回复
1 解答
1,628 次查看
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,629 次查看
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复