i.MX6DL - How many framebuffer can I use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL - How many framebuffer can I use?

1,280 Views
호영노
Contributor II

I used I.MX6DL. It has 1 IPU.

I used fb0 to camera output. and fb1 to QT's application area.

These are out put to LVDS. 

And I can mirroring the fb0 or fb1 to fb2. fb2 is output to External monitor. 

But I need 2 of framebuffer (fb0 and fb1 ) output to external monitor.

Is there any method to adding the 1 more framebuffer(fb3) in i.MX6DL ? 

Thanks.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,209 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the topic as below, hope helpful for you

https://community.nxp.com/message/834962?commentID=834962#comment-834962 

0 Kudos
Reply