i.MX6 vpu firmware source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 vpu firmware source code

3,160件の閲覧回数
teranishi_kenji
Contributor I

Hi all,

I are developing an encoding application on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga).

I would like to change rate control (quant param control) of macro-block level.

I think that it is necessary to change the firmware of the VPU. But, there are only a binary file (vpu_fw_imx6q.bin) of the firmware in yocto project.

Can I get the source code of VPU firmware or sample code from somewhere?

Best Regards,

Kenji

0 件の賞賛
返信
2 返答(返信)

2,218件の閲覧回数
teranishi_kenji
Contributor I

Hello Gusarambula,

Thank you for your comment.

I saw the API. However, there are no macro-block level API.

In other words, are there no method for setting macro-block's quant param?

BR,

0 件の賞賛
返信

2,218件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji Teranishi,

Unfortunately only the binaries are provided but an API is provided in order to work with the VPU firmware. You may find the following thread useful:

https://community.freescale.com/message/397728

I hope this helps!

Regards,

0 件の賞賛
返信