Can IMX6UL run on Android?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can IMX6UL run on Android?

2,261 Views
robinkwek
Contributor I

Hi,

Can i.MX6 UltraLite run on Android?

If yes, what is the memory size needed?

Labels (2)
0 Kudos
Reply
1 Reply

1,454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robin

one can look at  porting Android for i.MX28 EVK (128MB)

http://markdingst.blogspot.com/2011_07_01_archive.html  

In general hw acceleration is mandatory for Android (note, UL has

not gpu), as some api's may require support for hw acceleration.

Without gpu only the basic UI may be usable.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply