iMX6 Open-Drain maximum rating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Open-Drain maximum rating

3,106件の閲覧回数
erezsteinberg
Contributor IV

Hello experts,

I want to connect a PWM output using open-drain pad configuration.  The PWM bank voltage is 1.8V.

I couldn't find the information I need in the datasheet.

Can anyone answer :

1. In open-drain configuration, what is the maximum allowed external voltage on the pad?

2. What is the maximum allowed current through the internal transistor?

Regards,

Erez

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,796件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erez

1.  maximum allowed voltage on the pad is defined by

Datasheet Table 4. Absolute Maximum Ratings

Input/output voltage range :  OVDD+0.3V   (OVDD is the I/O supply voltage.)

2. maximum allowed current through the output transistor is not defined by

datasheet. Limitation would be max. Junction temperature defined in

Table 6. Operating Ranges

Note output transistor impedance may be affected by DSE, defined in

Table 33,34 GPIO Output Buffer Average Impedance

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,796件の閲覧回数
erezsteinberg
Contributor IV

Hi Igor,

Thanks for the prompt reply.

I saw the OVDD+0.3 spec in the Absolute Maximum Ratings table. However, I have doubt that it is correct for Open-Drain configuration.  I think OVDD+0.3 is the limit for Totem-Pole configuration.

Open-Drain is used very frequently for simple level-shifting is slow signals. I need to upshift from 1.8V to 3.3V.

Any way to verify this with the h/w team?

Regards,

Erez

0 件の賞賛
返信

2,796件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erez

yes this is correct. Note also there is esd protection

diode on pad.

Best regards

igor

0 件の賞賛
返信