i.MX6 vpu firmware source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 vpu firmware source code

3,184 Views
teranishi_kenji
Contributor I

Hi all,

I are developing an encoding application on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga).

I would like to change rate control (quant param control) of macro-block level.

I think that it is necessary to change the firmware of the VPU. But, there are only a binary file (vpu_fw_imx6q.bin) of the firmware in yocto project.

Can I get the source code of VPU firmware or sample code from somewhere?

Best Regards,

Kenji

0 Kudos
Reply
2 Replies

2,242 Views
teranishi_kenji
Contributor I

Hello Gusarambula,

Thank you for your comment.

I saw the API. However, there are no macro-block level API.

In other words, are there no method for setting macro-block's quant param?

BR,

0 Kudos
Reply

2,242 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji Teranishi,

Unfortunately only the binaries are provided but an API is provided in order to work with the VPU firmware. You may find the following thread useful:

https://community.freescale.com/message/397728

I hope this helps!

Regards,

0 Kudos
Reply