i.MX6 u-boot -- question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 u-boot -- question

1,650 Views
leerobert
Contributor I

Hello , I got 2 questions:

1. when to use u-boot.bin and when to use u-boot.imx ?

2. how to dump u-boot.bin and u-boot.imx, which tool should I learn to use ? Can you show me an example?

Labels (3)
0 Kudos
Reply
2 Replies

1,306 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lee

please look

u-boot.bin and u-boot.imx

https://community.freescale.com/message/464803#comment-464803

for usage please refer to BSP documentation, what BSP are you using ?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,306 Views
leerobert
Contributor I

I git cloned git://git.freescale.com/imx/uboot-imx.git

but I can't find a  tool to dump u-boot.bin in it.

0 Kudos
Reply