i.MX6 series DDR complete byte lane swapping.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 series DDR complete byte lane swapping.

跳至解决方案
1,348 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 Series DDR design.

Please see chapter 2.5.1 in IMX6SLHDG Rev.1.

It says as below.

=====

• JEDEC DDR3 memory restrictions are:

– No restrictions for complete byte lane swapping

– DQS and DQM must follow lanes

=====

I don't understand the meaning of the above "complete byte lane swapping".

It supports the swapping as the following image?

Complete_byte_lane_swapping.png

Best Regards,

Satoshi Shimoda

标签 (6)
标记 (1)
0 项奖励
回复
1 解答
1,077 次查看
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

I think you are right and also DQS and DQM must follow lanes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,078 次查看
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

I think you are right and also DQS and DQM must follow lanes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复