i.MX6 series DDR complete byte lane swapping.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 series DDR complete byte lane swapping.

ソリューションへジャンプ
1,352件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 Series DDR design.

Please see chapter 2.5.1 in IMX6SLHDG Rev.1.

It says as below.

=====

• JEDEC DDR3 memory restrictions are:

– No restrictions for complete byte lane swapping

– DQS and DQM must follow lanes

=====

I don't understand the meaning of the above "complete byte lane swapping".

It supports the swapping as the following image?

Complete_byte_lane_swapping.png

Best Regards,

Satoshi Shimoda

ラベル(6)
タグ(1)
0 件の賞賛
返信
1 解決策
1,081件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

I think you are right and also DQS and DQM must follow lanes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,082件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

I think you are right and also DQS and DQM must follow lanes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信