i.MX6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 processor

1,265 Views
kapilkumar
Contributor III

Hi Friends

can anyone tell me what is the total number of GPIO pins in i.MX6 processor (SABRE Board for Smart Devices)?

And what is the cost of  SABRE Board for Smart Devices??

Thanks & Regards,

Mr. Kapil

0 Kudos
Reply
1 Reply

1,211 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kapil

for price please look at Sabre SD product page, press "Buy" link

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Documentat...

i.MX6QD,SDL have 7 GPIO modules, 32 bits each (one bit corresponds to one GPIO signal).

Details can be found in sect.4.1.1 Pin Assignments i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

There is configuration tool for the i.MX family of processors which

contains pin settings and provides an easy way to configure pin signals.

Processor Expert for i.MX|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply