i.MX6 internal pullup tolerance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 internal pullup tolerance

1,329 次查看
dirkschäfer
Contributor III

Hello,

doeas somebody knows how large the tolerance of the internal pullups is? Every GPIO can be configured with 22k, 47 or 100k pullup. Tolerance?

Need this for a filtering RC.

Thanks for your help.

标签 (1)
0 项奖励
回复
1 回复

1,248 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dirk

tolerance of the pullups is +-20%.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------