i.MX6 internal pullup tolerance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 internal pullup tolerance

448 Views
dirkschäfer
Contributor III

Hello,

doeas somebody knows how large the tolerance of the internal pullups is? Every GPIO can be configured with 22k, 47 or 100k pullup. Tolerance?

Need this for a filtering RC.

Thanks for your help.

Labels (1)
0 Kudos
1 Reply

367 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dirk

tolerance of the pullups is +-20%.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------