i.MX6 failed DRAM address decode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 failed DRAM address decode

跳至解决方案
1,705 次查看
Kazuma_Sasaki
Senior Contributor I

Hi, 

We are making a product with i.MX6S. However, In rare case, we are encountering DDR accessing error.
therefore, we would like to identify failing point in DRAM chip for quality point of view.

It is need the failed address convert to ROW-COLUMN-BANK.

According to description from table 45-5 in reference manual rev 4, 07/2018.

Accessing address is able to decode by following mapping table.

pastedImage_3.png

If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right? pastedImage_4.png

Here is our error log getting from DDR stress test tool.

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 32, bank num: 8
Row size: 13, col size: 10
Chip select CSD0 is used
Density per chip select: 256MB
============================================
DDR Stress Test Iteration 1
Current Temperature: 46
============================================

DDR Freq: 396 MHz
t0.1: data is addr test
Address of failure(step2): 0x12001240
Data was: 0x52001240
But pattern should match address
Error: failed to run stress test!!!

Best Regards,

Kazuma Sasaki.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,626 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma 

>If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right?

yes this decoding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,627 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma 

>If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right?

yes this decoding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,626 次查看
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your quickly support.

Best Regards,

Kazuma Sasaki.

0 项奖励
回复