i.MX6 eMMCv4.41 fast boot support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 eMMCv4.41 fast boot support?

Jump to solution
2,916 Views
mehmetertugafsi
Contributor II

Hello,

In iMX6QD RM it says

"Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41" and

also it says in boot section :

Boot code supports following standards.

• MMCv4.4 or less

• eMMCv4.4 or less

• SDv2.0 or less

• eSDv2.10 rev-0.9, with or without FAST_BOOT.

• SDXCv3.0

Two different statements above made me confused. The question is can i use eMMCv4.41 for fast boot mode of i.mx6?

Thanks in advance..

Labels (5)
Tags (2)
0 Kudos
Reply
1 Solution
2,614 Views
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM supports eMMC version 4.41 for fast boot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)

View solution in original post

0 Kudos
Reply
4 Replies
2,614 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 supports fast boot, as it is stated in section 67.4.9 (MMC fast boot)

of the i.MX6 DQ Reference Manual.

Best regards

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,614 Views
mehmetertugafsi
Contributor II

Yes, it is apparent that it supports MMC fast boot but the question is whether e.MMC version 4.41 is supported for fast boot.

0 Kudos
Reply
2,615 Views
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM supports eMMC version 4.41 for fast boot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)

0 Kudos
Reply
2,614 Views
mehmetertugafsi
Contributor II

Ok thank you very much, i guess freescale should update the reference manuel and datasheet with the supoorted eMMC versions.

0 Kudos
Reply