i.MX6 eMMCv4.41 fast boot support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 eMMCv4.41 fast boot support?

ソリューションへジャンプ
2,860件の閲覧回数
mehmetertugafsi
Contributor II

Hello,

In iMX6QD RM it says

"Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41" and

also it says in boot section :

Boot code supports following standards.

• MMCv4.4 or less

• eMMCv4.4 or less

• SDv2.0 or less

• eSDv2.10 rev-0.9, with or without FAST_BOOT.

• SDXCv3.0

Two different statements above made me confused. The question is can i use eMMCv4.41 for fast boot mode of i.mx6?

Thanks in advance..

ラベル(5)
タグ(2)
0 件の賞賛
返信
1 解決策
2,558件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM supports eMMC version 4.41 for fast boot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,558件の閲覧回数
Yuri
NXP Employee
NXP Employee

The i.MX6 supports fast boot, as it is stated in section 67.4.9 (MMC fast boot)

of the i.MX6 DQ Reference Manual.

Best regards

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,558件の閲覧回数
mehmetertugafsi
Contributor II

Yes, it is apparent that it supports MMC fast boot but the question is whether e.MMC version 4.41 is supported for fast boot.

0 件の賞賛
返信
2,559件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM supports eMMC version 4.41 for fast boot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)

0 件の賞賛
返信
2,558件の閲覧回数
mehmetertugafsi
Contributor II

Ok thank you very much, i guess freescale should update the reference manuel and datasheet with the supoorted eMMC versions.

0 件の賞賛
返信