i.MX6 eCSPI Write/Read Timing Understanding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 eCSPI Write/Read Timing Understanding

Jump to solution
2,114 Views
chris_lambrecht
Contributor III

In looking at the Electrical Characteristics for the i.MX6 ULL processor (IMX6ULLCED PDF), Figure 35 and Table 47 indicate that there is a SPI Write timing of 15ns while there is a SPI Read Timing of 43ns (CS1) in Master Mode.

I read this to mean that the MISO data will not be registered correctly by the i.MX6 ULL processor if the i.MX6 is generating a SPI SCLK at a frequency greater than 23MHz (43ns). Therefore, if the i.MX6 wants to be able to register MISO data correctly, it must always run with a SPI clock slower than 43ns, or change between a faster clock when it doesn't care about the MISO data and a slower clock, when it does care to receive valid data.

Is this a correct understanding of these two timing parameters?

Thanks,

Chris

Labels (1)
0 Kudos
Reply
1 Solution
2,108 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chris

 

yes your understanding is correct.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
2,103 Views
chris_lambrecht
Contributor III

Thanks!!

0 Kudos
Reply
2,109 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chris

 

yes your understanding is correct.

 

Best regards
igor

0 Kudos
Reply