i.MX6 device tree of Linux Yocto BSP can set audmux connection?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 device tree of Linux Yocto BSP can set audmux connection?

跳至解决方案
1,654 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about device tee of i.MX6 Linux BSP (L3.14.28_1.0.0-ga).

I think device tree includes each module setting.

Then, I want to know whether device tree can set audiomux connection also.

(e.g. SSI1 --> AUDMUX port1 --(Internal Network Mode)--> AUDMUX port 4 )

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1 解答
1,256 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I think you can take the dtsi file in the BSP for reference.

e.g. imx6qdl-sabresd.dtsi. mux-int-port and mux-ext-port is used to set the AUDMUX in/out port number.

under the :

     sound {    

                    compatible = "fsl,imx6q-sabresd-wm8962",

                    ...

                    ...

                    ...

                    mux-int-port = <2>;

                    mux-ext-port = <3>;

For more details, please read the linux documentation. Documentation/devicetree/bindings/sound/imx-audio-wm8962.txt

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,257 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I think you can take the dtsi file in the BSP for reference.

e.g. imx6qdl-sabresd.dtsi. mux-int-port and mux-ext-port is used to set the AUDMUX in/out port number.

under the :

     sound {    

                    compatible = "fsl,imx6q-sabresd-wm8962",

                    ...

                    ...

                    ...

                    mux-int-port = <2>;

                    mux-ext-port = <3>;

For more details, please read the linux documentation. Documentation/devicetree/bindings/sound/imx-audio-wm8962.txt

0 项奖励
回复