i.MX6 device tree of Linux Yocto BSP can set audmux connection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 device tree of Linux Yocto BSP can set audmux connection?

ソリューションへジャンプ
1,653件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about device tee of i.MX6 Linux BSP (L3.14.28_1.0.0-ga).

I think device tree includes each module setting.

Then, I want to know whether device tree can set audiomux connection also.

(e.g. SSI1 --> AUDMUX port1 --(Internal Network Mode)--> AUDMUX port 4 )

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1 解決策
1,255件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can take the dtsi file in the BSP for reference.

e.g. imx6qdl-sabresd.dtsi. mux-int-port and mux-ext-port is used to set the AUDMUX in/out port number.

under the :

     sound {    

                    compatible = "fsl,imx6q-sabresd-wm8962",

                    ...

                    ...

                    ...

                    mux-int-port = <2>;

                    mux-ext-port = <3>;

For more details, please read the linux documentation. Documentation/devicetree/bindings/sound/imx-audio-wm8962.txt

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,256件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can take the dtsi file in the BSP for reference.

e.g. imx6qdl-sabresd.dtsi. mux-int-port and mux-ext-port is used to set the AUDMUX in/out port number.

under the :

     sound {    

                    compatible = "fsl,imx6q-sabresd-wm8962",

                    ...

                    ...

                    ...

                    mux-int-port = <2>;

                    mux-ext-port = <3>;

For more details, please read the linux documentation. Documentation/devicetree/bindings/sound/imx-audio-wm8962.txt

0 件の賞賛
返信