i.MX6 broken up DDR byte lane swapping

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 broken up DDR byte lane swapping

跳至解决方案
1,217 次查看
henfos
Contributor I

Hi,

According to "Routing considerations" in the hardware development guide to i.MX6 says it supports complete byte lane swapping. Does this also apply to broken up DDR byte lane swapping, as shown underneath:

pastedImage_1.png

Also the note in this subsection mentions that "target DDR IC register read value must be
transposed according to the data line swapping", can someone elaborate on the meaning of this?

标签 (2)
0 项奖励
回复
1 解答
1,002 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Henrik

no, " broken up" as shown on image is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,003 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Henrik

no, " broken up" as shown on image is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------