i.MX6 broken up DDR byte lane swapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 broken up DDR byte lane swapping

ソリューションへジャンプ
1,216件の閲覧回数
henfos
Contributor I

Hi,

According to "Routing considerations" in the hardware development guide to i.MX6 says it supports complete byte lane swapping. Does this also apply to broken up DDR byte lane swapping, as shown underneath:

pastedImage_1.png

Also the note in this subsection mentions that "target DDR IC register read value must be
transposed according to the data line swapping", can someone elaborate on the meaning of this?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,001件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Henrik

no, " broken up" as shown on image is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,002件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Henrik

no, " broken up" as shown on image is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------