i.MX6 boot appear "ECC error" information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 boot appear "ECC error" information

1,502件の閲覧回数
jackjiang
Contributor II

Dear,

The following information appears at startup. How to solve it? Thanks.

11.jpg

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,399件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jack

seems image is corrupted, probably due to sudden powering off during nand operations.

One can try to reprogram image using mfg tool from link

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,399件の閲覧回数
jackjiang
Contributor II

Thanks igor,

You are right, the issue was solved after reprogram image using mfg tool, but this method is too troublesome, whether there are other solutions, such as operating through Uboot.

0 件の賞賛
返信