i.MX6 boot appear "ECC error" information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 boot appear "ECC error" information

1,456 Views
jackjiang
Contributor II

Dear,

The following information appears at startup. How to solve it? Thanks.

11.jpg

Labels (1)
0 Kudos
Reply
2 Replies

1,353 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jack

seems image is corrupted, probably due to sudden powering off during nand operations.

One can try to reprogram image using mfg tool from link

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,353 Views
jackjiang
Contributor II

Thanks igor,

You are right, the issue was solved after reprogram image using mfg tool, but this method is too troublesome, whether there are other solutions, such as operating through Uboot.

0 Kudos
Reply