Hi,
When I run any X11 demo application I get a "Segmentation Fault" error. Please see log attached.
Does any one can help me?
console:
X.Org X Server 1.16.1
Release Date: 2014-09-21
X Protocol Version 11, Revision 0
Build Operating System: Linux 3.13.0-24-generic x86_64
Current Operating System: Linux imx6qsabresd 3.10.53-1.1.0_ga+g496fbe0 #4 SMP PREEMPT Mon Jun 15 12:08:25 JST 2015 armv7l
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24,bpp=32 ldb=spl1
Build Date: 26 May 2015 06:16:35PM
Current version of pixman: 0.32.4
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.1.log", Time: Wed Jun 24 10:57:34 2015
(==) Using config file: "/etc/X11/xorg.conf"
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
xinit: Unable to run program "xterm": No such file or directory
Specify a program on the command line or make sure that /usr/bin
is in your path.
xinit: connection to X server lost
waiting for X server to shut down (EE) Server terminated successfully (0). Closing log file.
Poky (Yocto Project Reference Distro) 1.6.2 imx6qsabresd /dev/ttymxc0
Xorg.log:
[475291.213]
X.Org X Server 1.16.1
Release Date: 2014-09-21
[475291.213] X Protocol Version 11, Revision 0
[475291.213] Build Operating System: Linux 3.13.0-24-generic x86_64
[475291.213] Current Operating System: Linux imx6qsabresd 3.10.53-1.1.0_ga+g496fbe0 #4 SMP PREEMPT Mon Jun 15 12:08:25 JST 2015 armv7l
[475291.214] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24,bpp=32 ldb=spl1
[475291.214] Build Date: 26 May 2015 06:16:35PM
[475291.214]
[475291.214] Current version of pixman: 0.32.4
[475291.214] Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
[475291.214] Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
[475291.214] (==) Log file: "/var/log/Xorg.0.log", Time: Mon Jun 22 17:32:48 2015
[475291.218] (==) Using config file: "/etc/X11/xorg.conf"
[475291.218] (==) Using system config directory "/usr/share/X11/xorg.conf.d"
[475291.220] (==) No Layout section. Using the first Screen section.
[475291.220] (==) No screen section available. Using defaults.
[475291.220] (**) |-->Screen "Default Screen Section" (0)
[475291.220] (**) | |-->Monitor "<default monitor>"
[475291.224] (==) No device specified for screen "Default Screen Section".
Using the first device section listed.
[475291.224] (**) | |-->Device "i.MX Accelerated Framebuffer Device"
[475291.224] (==) No monitor specified for screen "Default Screen Section".
Using a default monitor configuration.
[475291.224] (**) Option "BlankTime" "0"
[475291.225] (**) Option "StandbyTime" "0"
[475291.225] (**) Option "SuspendTime" "0"
[475291.225] (**) Option "OffTime" "0"
[475291.225] (==) Automatically adding devices
[475291.225] (==) Automatically enabling devices
[475291.225] (==) Automatically adding GPU devices
[475291.229] (WW) The directory "/usr/share/fonts/X11/TTF/" does not exist.
[475291.229] Entry deleted from font path.
[475291.229] (WW) The directory "/usr/share/fonts/X11/OTF/" does not exist.
[475291.229] Entry deleted from font path.
[475291.229] (WW) The directory "/usr/share/fonts/X11/Type1/" does not exist.
[475291.229] Entry deleted from font path.
[475291.231] (==) FontPath set to:
/usr/share/fonts/X11/misc/,
/usr/share/fonts/X11/100dpi/,
/usr/share/fonts/X11/75dpi/
[475291.231] (==) ModulePath set to "/usr/lib/xorg/modules"
[475291.231] (II) The server relies on udev to provide the list of input devices.
If no devices become available, reconfigure udev or disable AutoAddDevices.
[475291.231] (II) Loader magic: 0x1b3a20
[475291.231] (II) Module ABI versions:
[475291.231] X.Org ANSI C Emulation: 0.4
[475291.231] X.Org Video Driver: 18.0
[475291.231] X.Org XInput driver : 21.0
[475291.232] X.Org Server Extension : 8.0
[475291.240] (EE) systemd-logind: failed to get session: The name org.freedesktop.login1 was not provided by any .service files
[475291.241] (II) xfree86: Adding drm device (/dev/dri/card0)
[475291.242] (II) no primary bus or device found
[475291.242] falling back to /sys/devices/platform/Vivante GCCore/drm/card0
[475291.242] (II) LoadModule: "glx"
[475291.248] (II) Loading /usr/lib/xorg/modules/extensions/libglx.so
[475291.299] (II) Module glx: vendor="X.Org Foundation"
[475291.299] compiled for 1.16.1, module version = 1.0.0
[475291.299] ABI class: X.Org Server Extension, version 8.0
[475291.299] (==) AIGLX enabled
[475291.299] (II) LoadModule: "vivante"
[475291.300] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so
[475291.309] (II) Module vivante: vendor="X.Org Foundation"
[475291.309] compiled for 1.16.1, module version = 1.0.0
[475291.309] Module class: X.Org Video Driver
[475291.309] ABI class: X.Org Video Driver, version 18.0
[475291.309] (II) VIVANTE: driver for vivante fb: VivanteGC500, VivanteGC2100,
VivanteGCCORE
[475291.309] (--) using VT number 1
[475291.409] (WW) Falling back to old probe method for vivante
[475291.409] (II) Loading sub module "fbdevhw"
[475291.409] (II) LoadModule: "fbdevhw"
[475291.409] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so
[475291.419] (II) Module fbdevhw: vendor="X.Org Foundation"
[475291.419] compiled for 1.16.1, module version = 0.0.2
[475291.419] ABI class: X.Org Video Driver, version 18.0
[475291.419] (II) VIVANTE(0): using default device
[475291.419] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support
[475291.419] (II) VIVANTE(0): Device preferred mode 'fb0':U:1920x1080p-56
[475291.420] (II) VIVANTE(0): Creating default Display subsection in Screen section
"Default Screen Section" for depth/fbbpp 24/32
[475291.420] (==) VIVANTE(0): Depth 24, (==) framebuffer bpp 32
[475291.420] (==) VIVANTE(0): RGB weight 888
[475291.420] (==) VIVANTE(0): Default visual is TrueColor
[475291.420] (==) VIVANTE(0): Using gamma correction (1.0, 1.0, 1.0)
[475291.420] (**) VIVANTE(0): Option "fbdev" "/dev/fb0"
[475291.420] (II) VIVANTE(0): checking modes against framebuffer device...
[475291.420] (II) VIVANTE(0): checking modes against monitor...
[475291.420] (II) VIVANTE(0): Use built in mode (bpp 32)
[475291.420] (--) VIVANTE(0): Virtual size is 0x0 (pitch 0)
[475291.420] (==) VIVANTE(0): DPI set to (96, 96)
[475291.420] (II) Loading sub module "fb"
[475291.420] (II) LoadModule: "fb"
[475291.420] (II) Loading /usr/lib/xorg/modules/libfb.so
[475291.425] (II) Module fb: vendor="X.Org Foundation"
[475291.425] compiled for 1.16.1, module version = 1.0.0
[475291.425] ABI class: X.Org ANSI C Emulation, version 0.4
[475291.425] (II) Loading sub module "exa"
[475291.425] (II) LoadModule: "exa"
[475291.425] (II) Loading /usr/lib/xorg/modules/libexa.so
[475291.428] (II) Module exa: vendor="X.Org Foundation"
[475291.428] compiled for 1.16.1, module version = 2.6.0
[475291.428] ABI class: X.Org Video Driver, version 18.0
[475291.555] (II) VIVANTE(0): printing discovered frame buffer 'fb0' supported modes:
[475291.555] (II) VIVANTE(0): Modeline "U:1920x1080p-56"x0.0 130.00 1920 1960 1970 2070 1080 1083 1085 1115 -hsync -vsync -csync (62.8 kHz eP)
[475291.147] (II) VIVANTE(0): Output DISP4 BG has no monitor section
[475291.147] (II) VIVANTE(0): Printing probed modes for output DISP4 BG
[475291.147] (II) VIVANTE(0): Modeline "U:1920x1080p-56"x56.3 130.00 1920 1960 1970 2070 1080 1083 1085 1115 -hsync -vsync -csync (62.8 kHz eP)
[475291.147] (II) VIVANTE(0): Output DISP4 BG connected
[475291.147] (II) VIVANTE(0): Using exact sizes for initial modes
[475291.147] (II) VIVANTE(0): Output DISP4 BG using initial mode U:1920x1080p-56
[475291.147] (II) VIVANTE(0): imxDisplayPreInit: virtual set 1920 x 1080, display width 0
[475291.147] (II) VIVANTE(0): FBDevPreInit: adjust display width 1920
[475291.147] (**) VIVANTE(0): PreInit done
[475291.147] (--) Depth 24 pixmap format is 32 bpp
[475291.147] (II) VIVANTE(0): Init mode for fb device
[475291.195] (II) VIVANTE(0): hardware: DISP4 BG (video memory: 16335kB)
[475291.196] (II) VIVANTE(0): FB Start = 0x75726000 FB Base = 0x75726000 FB Offset = (nil) FB PhyBase 0x45200000
[475291.196] (II) VIVANTE(0): reserve 8355840 bytes for on screen frame buffer; total fb memory size 16727040 bytes; offset of shadow buffer 8355840
[475291.247] (II) VIVANTE(0): hardware: DISP4 BG (video memory: 16335kB)
[475291.287] (II) VIVANTE(0): test Initializing EXA
[475291.287] (II) VIVANTE(0): (driver build from: -dirty)
[475291.291] (II) EXA(0): Driver allocated offscreen pixmaps
[475291.291] (II) EXA(0): Driver registered support for the following operations:
[475291.291] (II) Solid
[475291.291] (II) Copy
[475291.291] (II) Composite (RENDER acceleration)
[475291.291] (II) UploadToScreen
[475291.310] (II) VIVANTE(0): Init SHM pixmap support
[475291.310] (==) VIVANTE(0): Backing store enabled
[475291.313] (==) VIVANTE(0): DPMS enabled
[475291.313] (II) VIVANTE(0): RandR 1.2 enabled, ignore the following RandR disabled message.
[475291.314] drmOpenDevice: node name is /dev/dri/card0
[475291.315] drmOpenDevice: open result is 13, (OK)
[475291.315] drmOpenDevice: node name is /dev/dri/card0
[475291.315] drmOpenDevice: open result is 13, (OK)
[475291.315] drmOpenByBusid: Searching for BusID platform:Vivante GCCore:00
[475291.315] drmOpenDevice: node name is /dev/dri/card0
[475291.315] drmOpenDevice: open result is 13, (OK)
[475291.315] drmOpenByBusid: drmOpenMinor returns 13
[475291.315] drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore:00
[475291.315] (II) [drm] DRM interface version 1.4
[475291.315] (II) [drm] DRM open master succeeded.
[475291.315] (II) VIVANTE(0): [drm] Using the DRM lock SAREA also for drawables.
[475291.315] (II) VIVANTE(0): [drm] framebuffer handle = 0x45200000
[475291.316] (II) VIVANTE(0): [drm] added 1 reserved context for kernel
[475291.316] (II) VIVANTE(0): X context handle = 0x1
[475291.316] (II) VIVANTE(0): [drm] installed DRM signal handler
[475291.316] (II) VIVANTE(0): [DRI] installation complete
[475291.316] (--) RandR disabled
[475291.359] (II) AIGLX: Screen 0 is not DRI2 capable
[475291.359] (EE) AIGLX: reverting to software rendering
[475291.461] (II) AIGLX: Loaded and initialized swrast
[475291.461] (II) GLX: Initialized DRISWRAST GL provider for screen 0
[475291.464] (II) VIVANTE(0): Setting screen physical size to 508 x 285
[475291.685] (II) config/udev: Adding input device Xxxxxx XXX-XXxXxX (/dev/input/event2)
[475291.685] (**) Xxxxxx XXX-XXxXxX: Applying InputClass "evdev touchscreen catchall"
[475291.685] (II) LoadModule: "evdev"
[475291.685] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[475291.688] (II) Module evdev: vendor="X.Org Foundation"
[475291.689] compiled for 1.16.1, module version = 2.8.2
[475291.689] Module class: X.Org XInput Driver
[475291.689] ABI class: X.Org XInput driver, version 21.0
[475291.689] (II) Using input driver 'evdev' for 'Xxxxxx XXX-XXxXxX'
[475291.689] (**) Xxxxxx XXX-XXxXxX: always reports core events
[475291.689] (**) evdev: Xxxxxx XXX-XXxXxX: Device: "/dev/input/event2"
[475291.689] (II) evdev: Xxxxxx XXX-XXxXxX: Using mtdev for this device
[475291.689] (--) evdev: Xxxxxx XXX-XXxXxX: Vendor 0x1477 Product 0x1021
[475291.689] (--) evdev: Xxxxxx XXX-XXxXxX: Found absolute axes
[475291.689] (--) evdev: Xxxxxx XXX-XXxXxX: Found absolute multitouch axes
[475291.690] (II) evdev: Xxxxxx XXX-XXxXxX: No buttons found, faking one.
[475291.690] (--) evdev: Xxxxxx XXX-XXxXxX: Found x and y absolute axes
[475291.690] (--) evdev: Xxxxxx XXX-XXxXxX: Found absolute touchscreen
[475291.690] (II) evdev: Xxxxxx XXX-XXxXxX: Configuring as touchscreen
[475291.690] (**) evdev: Xxxxxx XXX-XXxXxX: YAxisMapping: buttons 4 and 5
[475291.690] (**) evdev: Xxxxxx XXX-XXxXxX: EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200
[475291.690] (**) Option "config_info" "udev:/sys/devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.3/1-1.3:1.0/input/input2/event2"
[475291.690] (II) XINPUT: Adding extended input device "Xxxxxx XXX-XXxXxX" (type: TOUCHSCREEN, id 6)
[475291.690] (II) evdev: Xxxxxx XXX-XXxXxX: initialized for absolute axes.
[475291.691] (**) Xxxxxx XXX-XXxXxX: (accel) keeping acceleration scheme 1
[475291.691] (**) Xxxxxx XXX-XXxXxX: (accel) acceleration profile 0
[475291.691] (**) Xxxxxx XXX-XXxXxX: (accel) acceleration factor: 2.000
[475291.691] (**) Xxxxxx XXX-XXxXxX: (accel) acceleration threshold: 4
[475291.692] (II) config/udev: Adding input device Xxxxxx XXX-XXxXxX (/dev/input/mouse1)
[475291.692] (II) No input driver specified, ignoring this device.
[475291.692] (II) This device may have been added with another device file.
[475291.694] (II) config/udev: Adding input device ELECOM ELECOM USB mouse with wheel (/dev/input/event0)
[475291.694] (**) ELECOM ELECOM USB mouse with wheel : Applying InputClass "evdev pointer catchall"
[475291.694] (II) Using input driver 'evdev' for 'ELECOM ELECOM USB mouse with wheel '
[475291.694] (**) ELECOM ELECOM USB mouse with wheel : always reports core events
[475291.694] (**) evdev: ELECOM ELECOM USB mouse with wheel : Device: "/dev/input/event0"
[475291.695] (--) evdev: ELECOM ELECOM USB mouse with wheel : Vendor 0x56e Product 0x1c
[475291.695] (--) evdev: ELECOM ELECOM USB mouse with wheel : Found 3 mouse buttons
[475291.695] (--) evdev: ELECOM ELECOM USB mouse with wheel : Found scroll wheel(s)
[475291.695] (--) evdev: ELECOM ELECOM USB mouse with wheel : Found relative axes
[475291.695] (--) evdev: ELECOM ELECOM USB mouse with wheel : Found x and y relative axes
[475291.695] (II) evdev: ELECOM ELECOM USB mouse with wheel : Configuring as mouse
[475291.695] (II) evdev: ELECOM ELECOM USB mouse with wheel : Adding scrollwheel support
[475291.695] (**) evdev: ELECOM ELECOM USB mouse with wheel : YAxisMapping: buttons 4 and 5
[475291.695] (**) evdev: ELECOM ELECOM USB mouse with wheel : EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200
[475291.695] (**) Option "config_info" "udev:/sys/devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.4/1-1.4.1/1-1.4.1:1.0/input/input0/event0"
[475291.695] (II) XINPUT: Adding extended input device "ELECOM ELECOM USB mouse with wheel " (type: MOUSE, id 7)
[475291.695] (II) evdev: ELECOM ELECOM USB mouse with wheel : initialized for relative axes.
[475291.695] (**) ELECOM ELECOM USB mouse with wheel : (accel) keeping acceleration scheme 1
[475291.696] (**) ELECOM ELECOM USB mouse with wheel : (accel) acceleration profile 0
[475291.696] (**) ELECOM ELECOM USB mouse with wheel : (accel) acceleration factor: 2.000
[475291.696] (**) ELECOM ELECOM USB mouse with wheel : (accel) acceleration threshold: 4
[475291.697] (II) config/udev: Adding input device ELECOM ELECOM USB mouse with wheel (/dev/input/mouse0)
[475291.697] (II) No input driver specified, ignoring this device.
[475291.697] (II) This device may have been added with another device file.
[475291.699] (II) config/udev: Adding input device Dell Dell USB Keyboard (/dev/input/event1)
[475291.699] (**) Dell Dell USB Keyboard: Applying InputClass "evdev keyboard catchall"
[475291.699] (II) Using input driver 'evdev' for 'Dell Dell USB Keyboard'
[475291.699] (**) Dell Dell USB Keyboard: always reports core events
[475291.699] (**) evdev: Dell Dell USB Keyboard: Device: "/dev/input/event1"
[475291.699] (--) evdev: Dell Dell USB Keyboard: Vendor 0x413c Product 0x2003
[475291.699] (--) evdev: Dell Dell USB Keyboard: Found keys
[475291.699] (II) evdev: Dell Dell USB Keyboard: Configuring as keyboard
[475291.699] (**) Option "config_info" "udev:/sys/devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.4/1-1.4.2/1-1.4.2:1.0/input/input1/event1"
[475291.699] (II) XINPUT: Adding extended input device "Dell Dell USB Keyboard" (type: KEYBOARD, id 8)
[475291.699] (**) Option "xkb_rules" "evdev"
[475291.699] (**) Option "xkb_model" "pc104"
[475291.699] (**) Option "xkb_layout" "us"
(EE)
(EE) Backtrace:
(EE)
(EE) Segmentation fault at address 0x68
(EE)
Fatal server error:
(EE) Caught signal 11 (Segmentation fault). Server aborting
(EE)
(EE)
Please consult the The X.Org Foundation support
at http://wiki.x.org
for help.
(EE) Please also check the log file at "/var/log/Xorg.0.log" for additional information.
(EE)
(EE) Server terminated with error (1). Closing log file.