i.MX6 Watchdog Timer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,182件の閲覧回数
morganbadgett
Contributor I

It appears from reading the Applications Processor Reference Manual for the i.MX6 Quad, that once the Watchdog Timer (WDOG) is enabled, it cannot be disabled until a POR has occurred.  Has anyone been successful in disabling the watchdog after it's been disabled, without going through a POR?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,378件の閲覧回数
art
NXP Employee
NXP Employee

There is no way to clear the Watchdog Enable (WDE) bit of the Watchdog Control Register (WCR) in software once it is set. Only the Power-On Reset or Watchdog Reset events can clear it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,379件の閲覧回数
art
NXP Employee
NXP Employee

There is no way to clear the Watchdog Enable (WDE) bit of the Watchdog Control Register (WCR) in software once it is set. Only the Power-On Reset or Watchdog Reset events can clear it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------