i.MX6 VDDSOC rush current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 VDDSOC rush current

ソリューションへジャンプ
1,766件の閲覧回数
torus1000
Contributor V

Hi,

I measured the current of my i.MX6 board then VDDSOC rush current observed roughly 6A on the way to ramp up around 1V.

Does anybody know it is normal or not? Please let me know which part consumes such big current?

Thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,610件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

max. currents are given in IMX6DQCEC  Table 8 "Maximum Supply Currents",

however at first moment of power-up these values may be significantly exceeded,

since power capacitors are charged and consume much current.

So this value depends on particular board and 6A may be considered

as also normal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,611件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

max. currents are given in IMX6DQCEC  Table 8 "Maximum Supply Currents",

however at first moment of power-up these values may be significantly exceeded,

since power capacitors are charged and consume much current.

So this value depends on particular board and 6A may be considered

as also normal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信