i.MX6 VDDSOC rush current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 VDDSOC rush current

跳至解决方案
1,753 次查看
torus1000
Contributor V

Hi,

I measured the current of my i.MX6 board then VDDSOC rush current observed roughly 6A on the way to ramp up around 1V.

Does anybody know it is normal or not? Please let me know which part consumes such big current?

Thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,597 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

max. currents are given in IMX6DQCEC  Table 8 "Maximum Supply Currents",

however at first moment of power-up these values may be significantly exceeded,

since power capacitors are charged and consume much current.

So this value depends on particular board and 6A may be considered

as also normal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,598 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

max. currents are given in IMX6DQCEC  Table 8 "Maximum Supply Currents",

however at first moment of power-up these values may be significantly exceeded,

since power capacitors are charged and consume much current.

So this value depends on particular board and 6A may be considered

as also normal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复