i.MX6 USB boot flow in serial downloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 USB boot flow in serial downloader

Jump to solution
2,332 Views
m_c
Senior Contributor I

In the figure 8-2 of i.MX6 Quad/Dual reference manual <http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf>, it shows USB boot flow. Is it only apply for BOOT_MODE[1:0]=01? Or also apply to enter serial downloader by boot fail from SPI NOR/eMMC/NAND/... in BOOT_MODE[1:0]=10?

pastedImage_150.png

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes this also applies when entering serial downloader by boot fail from

other modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes this also applies when entering serial downloader by boot fail from

other modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply