i.MX6 USB boot flow in serial downloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 USB boot flow in serial downloader

ソリューションへジャンプ
2,186件の閲覧回数
m_c
Senior Contributor I

In the figure 8-2 of i.MX6 Quad/Dual reference manual <http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf>, it shows USB boot flow. Is it only apply for BOOT_MODE[1:0]=01? Or also apply to enter serial downloader by boot fail from SPI NOR/eMMC/NAND/... in BOOT_MODE[1:0]=10?

pastedImage_150.png

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,284件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes this also applies when entering serial downloader by boot fail from

other modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,285件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes this also applies when entering serial downloader by boot fail from

other modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信