i.MX6 ULL eMMC has bit errors during 8 bit bus width

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 ULL eMMC has bit errors during 8 bit bus width

8,088件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

we have a custom board with i.MX6 ULL and Micron MTFC4GACAJCN-4M at usdhc2 (eMMC JEDEC 5.0) running under official FSL BSP 4.1.15-2.0.1. Using 4 bus width works perfectly in HS200 mode.

If i adjust the DTS to 8 bit bus width, i always got the following error and Linux switches back to 4 bit bus width:

mmc1: switch to bus width 2 failed

I investigated this issue and found out that mmc_compare_ext_csds() fails with error code -84 (EBADMSG). Then i dumped the EXT CSD register (dumps attached). If i compare both files i see a few bit errors in the 8 bit dump (at byte 19,157,184,196,213,214,231,241,247,487,488). These bit errors are the same over several boards (same layout).

This issue looks similiar to this, but we think the DAT lines are connected properly:

IMX6SX eMMC DDR with 8 bits bus problem 

Here are the relevant parts of the DT:

pinctrl_usdhc2_8bit: pinctrl_usdhc2_8bitGrp {
        fsl,pins = <
            MX6UL_PAD_CSI_VSYNC__USDHC2_CLK     0x10069
            MX6UL_PAD_CSI_HSYNC__USDHC2_CMD     0x17059
            MX6UL_PAD_CSI_DATA00__USDHC2_DATA0     0x17059
            MX6UL_PAD_CSI_DATA01__USDHC2_DATA1     0x17059
            MX6UL_PAD_CSI_DATA02__USDHC2_DATA2     0x17059
            MX6UL_PAD_CSI_DATA03__USDHC2_DATA3     0x17059
            MX6UL_PAD_CSI_DATA04__USDHC2_DATA4     0x17059
            MX6UL_PAD_CSI_DATA05__USDHC2_DATA5     0x17059
            MX6UL_PAD_CSI_DATA06__USDHC2_DATA6     0x17059
            MX6UL_PAD_CSI_DATA07__USDHC2_DATA7     0x17059
        >;
    };

    pinctrl_usdhc2_8bit_100MHz: pinctrl_usdhc2_8bit_100MHz_Grp {
        fsl,pins = <
            MX6UL_PAD_CSI_VSYNC__USDHC2_CLK     0x100b9     
            MX6UL_PAD_CSI_HSYNC__USDHC2_CMD     0x170b9
            MX6UL_PAD_CSI_DATA00__USDHC2_DATA0     0x170b9
            MX6UL_PAD_CSI_DATA01__USDHC2_DATA1     0x170b9
            MX6UL_PAD_CSI_DATA02__USDHC2_DATA2     0x170b9
            MX6UL_PAD_CSI_DATA03__USDHC2_DATA3     0x170b9
            MX6UL_PAD_CSI_DATA04__USDHC2_DATA4     0x170b9
            MX6UL_PAD_CSI_DATA05__USDHC2_DATA5     0x170b9
            MX6UL_PAD_CSI_DATA06__USDHC2_DATA6     0x170b9
            MX6UL_PAD_CSI_DATA07__USDHC2_DATA7     0x170b9
        >;
    };

    pinctrl_usdhc2_8bit_200MHz: pinctrl_usdhc2_8bit_200MHz_Grp {
        fsl,pins = <
            MX6UL_PAD_CSI_VSYNC__USDHC2_CLK     0x100f9
            MX6UL_PAD_CSI_HSYNC__USDHC2_CMD     0x170f9
            MX6UL_PAD_CSI_DATA00__USDHC2_DATA0     0x170f9
            MX6UL_PAD_CSI_DATA01__USDHC2_DATA1     0x170f9
            MX6UL_PAD_CSI_DATA02__USDHC2_DATA2     0x170f9
            MX6UL_PAD_CSI_DATA03__USDHC2_DATA3     0x170f9
            MX6UL_PAD_CSI_DATA04__USDHC2_DATA4     0x170f9
            MX6UL_PAD_CSI_DATA05__USDHC2_DATA5     0x170f9
            MX6UL_PAD_CSI_DATA06__USDHC2_DATA6     0x170f9
            MX6UL_PAD_CSI_DATA07__USDHC2_DATA7     0x170f9
        >;
    };


&usdhc2 {
     pinctrl-names = "default", "state_100mhz", "state_200mhz";
     pinctrl-0 = <&pinctrl_usdhc2_8bit>;
     pinctrl-1 = <&pinctrl_usdhc2_8bit_100MHz>;
     pinctrl-2 = <&pinctrl_usdhc2_8bit_200MHz>;
     bus-width = <8>;
     broken-cd;
     non-removable;
     status = "okay";
};‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Here is the debugfs output:

# cat /sys/kernel/debug/mmc1/ios
clock: 132000000 Hz
actual clock: 132000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 2 (4 bits)
timing spec: 9 (mmc HS200)
signal voltage: 0 (1.80 V)‍‍‍‍‍‍‍‍‍‍
ラベル(2)
タグ(2)
0 件の賞賛
返信
6 返答(返信)

7,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

one can try to adjust drive strength settings in pads associated

with problematic bits: SW_PAD_CTL_PAD_x_x SW PAD Control
Registers, Chapter 32 IOMUX Controller (IOMUXC) i.MX6ULL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

and control waveforms with oscilloscope.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,126件の閲覧回数
lategoodbye
Senior Contributor I

I tried the following settings, but the bit errors stays:

SDHCI frequency | DT PAD control | DSE

200 MHz | 170F9 | RO / 7

200 MHz | 170F1 | RO / 6

200 MHz | 170C9 | RO

50 MHz | 17079 | RO / 7

50 MHz | 17049 | RO

Could this be a clock domain crossing issue?

0 件の賞賛
返信

7,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

most likely this may be noise coupling issue. Is it working at lower frequencies?

Also may be useful to check layout, described in sect.3.6.8 High speed signal routing recommendations

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

All synchronous modules should have bus length matching and relative clock length control.
— For SD module interfaces:
– Match data and CMD trace lengths (length delta depends on bus rates)
– CLK should be longer than the longest signal in the Data/CMD group (+5 mils)
— Similar DDR rules must be followed for data, address and control as for SD module interfaces.

Best regards
igor

0 件の賞賛
返信

7,126件の閲覧回数
lategoodbye
Senior Contributor I

After fixing a probing issue of the sdhci driver for 1.8V only signal voltage, i was able to reduce the clock frequency:

After removing the pinctrl settings for 100MHz and 200MHz state in DT:
clock:          52000000 Hz
actual clock:   33000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      2 (4 bits)
timing spec:    8 (mmc DDR52)
signal voltage: 0 (1.80 V)

After additionaling setting the max-frequency to 20 MHz via DT:
clock:          20000000 Hz
actual clock:   16500000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      2 (4 bits)
timing spec:    8 (mmc DDR52)
signal voltage: 0 (1.80 V)

In both cases the issue still occured.‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 件の賞賛
返信

7,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please use logic analyzer and try to find source of error

mmc_compare_ext_csds() fails with error code -84 (EBADMSG), use

waveforms and descriptions in mmc specification JESD84-B50.

Also one can try with i.MX6ULL EVK.

Best regards
igor

0 件の賞賛
返信

7,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also one can test 8 bit mode in uboot:

uboot/board/freescale/mx6ullevk/mx6ullevk.c

use
#define CONFIG_MX6ULL_EVK_EMMC_REWORK

uboot-imx.git - Freescale i.MX u-boot Tree 

0 件の賞賛
返信