Hi everyone,
thanks to some help from some users here, I was able to change the i.MX UART driver so that I can send and receive 9-bit frames in "slave address normal detection" mode.
Detection of the address byte (first byte) of the message is working fine.
The problem I was unable to solve to my satisfaction is "resetting" the detection.
As stated in the user manual, the address byte (9th bit = 1) and all subsequent bytes are written into the RxFIFO - this works correctly. But how should I tell the controller, that one message is completely received and it should now wait for another address byte (9th bit = 1)?
Currently, I use the IDLE interrupt for this: When an IDLE is detected on the RX Line (after an address byte was received), then the message was received in full extent. So now, I disable the 9-bit mode (MDEN=0 to UMCR register) and directly enable 9-bit mode again (MDEN=1).
temp = readl(sport->port.membase + UMCR);
temp &= ~UMCR_MDEN; // disable 9-bit (MultiDrop) mode
writel(temp, sport->port.membase + UMCR);
temp |= UMCR_MDEN; // enable 9-bit (MultiDrop) mode
writel(temp, sport->port.membase + UMCR);
But I think this is not quite elegant.
Is there a better way to "reset" the slave address detection?
Thanks in advance