Where to find mfgtool version 2.7.0 for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to find mfgtool version 2.7.0 for Linux

4,420件の閲覧回数
mattia_maldini
Contributor II

Hello everyone,

I am working on a SOM with i.MX6UL on it. The customer support of the producer (wireless-tag) warned me that `uuu` (the latest evolution of mfgtools) is not supported to update the flash memory via USB, and that they instead use mfgtools version 2.7.0 .

I have visited the Github repository of mfgtools (GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. ), but the earliest version I can find is the 2.8.0 . Is there an archive where I can get that specific iteration?

Thanks for the assistance

ラベル(1)
タグ(1)
6 返答(返信)

4,115件の閲覧回数
mattia_maldini
Contributor II

Hello yuri,

Yes, that is indeed version 2.7, but for Windows. Unfortunately, I was looking for the Linux version.


In the meantime I figured out that the tool was probably never supported for Linux, let alone version 2.7 . The latest version on the branch linux is 2.3.4, and it fails to compile.

I will either use a virtual machine or an actual windows machine.

4,115件の閲覧回数
mattia_maldini
Contributor II

Hello Yuri,

That is marked as version 2.1 (both in the name of the package and in the Release Notes), I'm looking for 2.7. Is there a reason I shoudn't use such version?

0 件の賞賛
返信

4,114件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The Summary Page, mentioned above, contains many (archieve) MFG releases, which

were tested and used with corresponding Linux BSPs.   Just take MFG with needed NXP BSP

release.

Regards,

Yuri.

0 件の賞賛
返信

4,115件の閲覧回数
mattia_maldini
Contributor II

Hello Yuri,

I am unable to find the specific version I'm looking for, which is mfgtools 2.7 . I am looking for this specific version because it is the one the SOM vendor indicated as the one supported by its product.

Does such version exist? If it does, it is not present in the summary page. Is there any reason I cannot find that specific version? If so, I can inquire the vendor further or try a different version. Before that, however, I would like to know whether mfgtools version 2.7 is available.

0 件の賞賛
返信

4,115件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The following is MFG git.

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Sources of the 2.7 :

GitHub - NXPmicro/mfgtools at windows 

Regards,

Yuri.

0 件の賞賛
返信

4,115件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Please try the following package:

https://www.nxp.com/webapp/Download?colCode=IMX_L4.1.15_2.1.0_MFG_TOOL

Summary Page:

i.MX Software | NXP 

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信