i.MX6: Setting up lxc on imx6 and running android container on top of it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6: Setting up lxc on imx6 and running android container on top of it

2,355件の閲覧回数
bharaths
Contributor I

Hi,

I am checking the feasibility of enabling lxc(LinuX Container) in imx6d/imx6q with the latest kernel provided from Freescale.

Can anyone please provide me with the steps to achieve this?

Is it in-built in the kernel or do I need to enable it via menuconfig or do i need a patch for it?

Once lxc is setup, I would like to run android container on top it.

Has anyone successfully achieved this? Please share the steps to do it.

Regards,

Bharath S

タグ(3)
0 件の賞賛
返信
1 返信

1,570件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Dear Bharath,

You can review the following link:

LXC docker

And you can check this presentation, I founded very good

http://events.linuxfoundation.org/sites/events/files/slides/LXCBENCH_ALS2013-v1.00_0.pdf

0 件の賞賛
返信