i.MX6: Setting up lxc on imx6 and running android container on top of it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6: Setting up lxc on imx6 and running android container on top of it

2,293 Views
bharaths
Contributor I

Hi,

I am checking the feasibility of enabling lxc(LinuX Container) in imx6d/imx6q with the latest kernel provided from Freescale.

Can anyone please provide me with the steps to achieve this?

Is it in-built in the kernel or do I need to enable it via menuconfig or do i need a patch for it?

Once lxc is setup, I would like to run android container on top it.

Has anyone successfully achieved this? Please share the steps to do it.

Regards,

Bharath S

Tags (3)
0 Kudos
Reply
1 Reply

1,508 Views
jamesbone
NXP TechSupport
NXP TechSupport

Dear Bharath,

You can review the following link:

LXC docker

And you can check this presentation, I founded very good

http://events.linuxfoundation.org/sites/events/files/slides/LXCBENCH_ALS2013-v1.00_0.pdf

0 Kudos
Reply