i.MX6 SSI Operating Modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 SSI Operating Modes

1,551件の閲覧回数
m_c
Senior Contributor I

Which mode is used in i.MX6 SABRE-SD with WM8962?

Which mode is used in i.MX6 SABRE-AI with CS42888?

pastedImage_1.png

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,418件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

i.MX6 SABRE-SD uses SSI I2S slave with WM8962 and such

configuration is described in sect.61.8.1.4 I2S Mode i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

i.MX6 SABRE-AI with CS42888 does not use SSI, it uses another module - ESAI.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,418件の閲覧回数
m_c
Senior Contributor I

By dump SSIx_SCR can find out.

0 件の賞賛
返信