i.MX6 SSI Operating Modes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SSI Operating Modes

1,549 Views
m_c
Senior Contributor I

Which mode is used in i.MX6 SABRE-SD with WM8962?

Which mode is used in i.MX6 SABRE-AI with CS42888?

pastedImage_1.png

Labels (2)
0 Kudos
Reply
2 Replies

1,416 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

i.MX6 SABRE-SD uses SSI I2S slave with WM8962 and such

configuration is described in sect.61.8.1.4 I2S Mode i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

i.MX6 SABRE-AI with CS42888 does not use SSI, it uses another module - ESAI.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,416 Views
m_c
Senior Contributor I

By dump SSIx_SCR can find out.

0 Kudos
Reply