i.MX6 SDMA performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 SDMA performance

ソリューションへジャンプ
2,561件の閲覧回数
torus1000
Contributor V


Hi,

We applyed old i.MX6 ltib SDMA:ap_2_ap patch for yocto then it worked.
However, the performance is not enough for us. It was under 40MB/s.

(Please refer to https://community.freescale.com/message/353963#353963)

Do we have any way to improve the performance?

Thanks.

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,265件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,266件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信