i.MX6 SDMA performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 SDMA performance

跳至解决方案
1,722 次查看
torus1000
Contributor V


Hi,

We applyed old i.MX6 ltib SDMA:ap_2_ap patch for yocto then it worked.
However, the performance is not enough for us. It was under 40MB/s.

(Please refer to https://community.freescale.com/message/353963#353963)

Do we have any way to improve the performance?

Thanks.

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,426 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,427 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复