i.MX6 SDMA performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SDMA performance

Jump to solution
2,511 Views
torus1000
Contributor V


Hi,

We applyed old i.MX6 ltib SDMA:ap_2_ap patch for yocto then it worked.
However, the performance is not enough for us. It was under 40MB/s.

(Please refer to https://community.freescale.com/message/353963#353963)

Do we have any way to improve the performance?

Thanks.

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
2,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,216 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

40-60 MB/s is typical figure, so it can not be considered

as abnormal. Probably you can try to decrease number of running

applications, if possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply