i.MX6 SD2 Card Detect pin disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 SD2 Card Detect pin disable

跳至解决方案
2,949 次查看
vincentchou
Contributor IV

Hi!  friends,

Right now we designed a i.MX6 Solo board with a Wifi Module (RTL8189es) wired to the SD2 bus.  However, we did not know which SD2_CD_B pin should be used and our module does not require that pin either.  In that case, we let NANDF_D2 (used in the SABRESD EVB) and GPIO_4 (listed in the reference manual) float.  Later on we discovered that there is an error message output "uSDHC1: No card-detect pin available!" message on the boot log output.  In addition, the system seems to have to problem to recognize there is a Wifi module plugged into SD2 bus.  Is there anyway we could fix this by letting the system know the module is plugged in the software?  Any help is greatly appreciated!  We are running Android 4.0.4 on a board similar to i.MX6 Sabresd EVB.

Vincent

标签 (3)
1 解答
1,957 次查看
lily_zhang
NXP Employee
NXP Employee

You can check SDHC configuration in your board file

static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {

        .cd_gpio = SABRESD_SD2_CD,

        .wp_gpio = SABRESD_SD2_WP,

        .keep_power_at_suspend = 1,

        .support_8bit = 1,

        .delay_line = 0,

        .cd_type = ESDHC_CD_CONTROLLER,

        .runtime_pm = 1,

};

enum cd_types {

        ESDHC_CD_NONE,          /* no CD, neither controller nor gpio */

        ESDHC_CD_CONTROLLER,    /* mmc controller internal CD */

        ESDHC_CD_GPIO,          /* external gpio pin for CD */

        ESDHC_CD_PERMANENT,     /* no CD, card permanently wired to host */

};

You can consider set cd_type as ESDHC_CD_PERMANENT

在原帖中查看解决方案

2 回复数
1,958 次查看
lily_zhang
NXP Employee
NXP Employee

You can check SDHC configuration in your board file

static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {

        .cd_gpio = SABRESD_SD2_CD,

        .wp_gpio = SABRESD_SD2_WP,

        .keep_power_at_suspend = 1,

        .support_8bit = 1,

        .delay_line = 0,

        .cd_type = ESDHC_CD_CONTROLLER,

        .runtime_pm = 1,

};

enum cd_types {

        ESDHC_CD_NONE,          /* no CD, neither controller nor gpio */

        ESDHC_CD_CONTROLLER,    /* mmc controller internal CD */

        ESDHC_CD_GPIO,          /* external gpio pin for CD */

        ESDHC_CD_PERMANENT,     /* no CD, card permanently wired to host */

};

You can consider set cd_type as ESDHC_CD_PERMANENT

1,957 次查看
vincentchou
Contributor IV

HI!  Xiaoli,

Happy Chinese New Year!  We did follow the same configuration as EMMC and set the SD2.  Thanks a lot!

Vincent

0 项奖励
回复