i.MX6S 24MHz Oscillator Power Rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S 24MHz Oscillator Power Rating

1,224 Views
dvona
Contributor II

Greetings,

I have a quick question about the crystal oscillator needed for the i.MX6 Solo processor. 

We have reviewed the latest recomendations for the XTALI/XTALO clock input in the most recent hardware designer guide and the EB830 bulletin.  We understand the drive requirements for using a crystal have increased and have referenced the spreadsheet attached to EB830.

My question relates to using a straight oscillator connected to XTALI with XTALO left floating (which the documentation says is acceptable).  What I am wondering is this: if we are using a 24MHz oscillator (not a crystal) do the same maximum drive requirements apply?  In other words, could we simply use an oscillator like the CB3LV-3I-24M0000 which has a max drive of 100uW or would we need something more like a 250uW part?

Thanks,

-Dan

Labels (1)
0 Kudos
Reply
3 Replies

859 Views
SergioSolis
NXP Employee
NXP Employee

Hello Dan,

Yes, the same maximum drive requirements apply with an oscillator as with a crystal. You can use the 100uW just make sure 100% you wont drive more than that. Personally I would go with a 150uW.

0 Kudos
Reply

859 Views
amanda24
Contributor I

SerchMX,

Since there aren't any references to drive level with a standard oscillator, is there something else to go by to tell if it might work with the i.MX6 Solo processor?

Also, I have some concerns over the micro phonics & EMI/RFI susceptibility of the crystal.  Is there a particular reason why a crystal was chosen to run the processor, as opposed to just a regular oscillator?

0 Kudos
Reply

859 Views
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately we are having some delays in our responses since the Holidays in China, SergioSolis, it is reviewing this case. We will provide a response as soon as possible.

0 Kudos
Reply