i.MX6 SABRE Board for Smart Devices Linux Boot Fail Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 SABRE Board for Smart Devices Linux Boot Fail Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

1,873件の閲覧回数
mianbohuang
Contributor I

I burn my uboot image and kernel image ,file system using the "Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER"

but after rebooting from SD,it failed ,the uart output infor is as follows,there is a kernel panic info.

U-Boot 2009.08 (Aug 16 2013 - 12:04:20)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 187
Temperature: 37 C, calibration data 0x5a05017d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=11
Net: got MAC address from IIM: 00:04:9f:02:af:f3
FEC0 [PRIME]
Hit any key to stop autoboot: 0
mmc2 is current device

MMC read: dev # 2, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.15
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3355508 Bytes = 3.2 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 3.0.15 (hhj@ubuntu) (gcc version 4.6.3 20120105 (prerelease) (crosstool-NG linaro-1.13.1-2012.01-20120125 - Linaro GCC 2012.01) ) #1 SMP PREEMPT Sat Sep 12 17:13:36 CST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad Sabre-SD Board
Ignoring unrecognised tag 0x54410008
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 7 pages/cpu @8c008000 s5216 r8192 d15264 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 227328
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 640MB 256MB = 896MB total
Memory: 901740k/901740k available, 146836k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xf4600000 - 0xffe00000 ( 184 MB)
vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x80036000 ( 184 kB)
.text : 0x80036000 - 0x806048b8 (5947 kB)
.data : 0x80606000 - 0x8064da20 ( 287 kB)
.bss : 0x8064da44 - 0x80677e6c ( 170 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:496
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
cpaddr = c0840000 wait_iram_base=c0812000
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2800 <--> 3150 mV at 3000 mV fast normal
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
IMX usb wakeup probe
IMX usb wakeup probe
bio: create slab <bio-0> at 0
print_constraints: VDDA: 2500 mV
print_constraints: VDDIO: 3300 mV
machine_constraints_voltage: VDDD: unsupportable voltage constraints
reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22
reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
add wake up source irq 75
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: PFUZE100_SW1A: 650 <--> 1437 mV at 1187 mV
print_constraints: PFUZE100_SW1B: 650 <--> 1437 mV at 650 mV
print_constraints: PFUZE100_SW1C: 650 <--> 1437 mV at 1187 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 400 <--> 1975 mV at 1575 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 1200 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 1200 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource mxc_timer1
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode: dummy_timer is not functional.
Clockevents: could not switch to one-shot mode:
Could not switch to high resolution mode on CPU 2
dummy_timer is not functional.
Clockevents: could not switch to one-shot mode:
Could not switch to high resolution mode on CPU 0
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Bus freq driver module loaded
Static Power Management for Freescale i.MX6
cpaddr = c0841000 suspend_iram_base=c08ea000
PM driver module loaded
i.MXC CPU frequency driver
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 1761
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 3
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi
mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
imx-ipuv3 imx-ipuv3.0: Channel already disabled 9
imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 9
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 240x67
imx-ipuv3 imx-ipuv3.0: Channel already disabled 10
imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 10
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.1: Channel already disabled 9
imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 9
imx-ipuv3 imx-ipuv3.1: Channel already disabled 10
imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 10
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb
imx-ipuv3 imx-ipuv3.1: Channel already disabled 7
imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 7
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.3: ipu1-di1 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
Can't recover from RESET HBA!
No sata disk.
m25p80 spi0.0: found m25p05-nonjedec, expected sst25vf016b
m25p80 spi0.0: m25p05-nonjedec (64 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "bootloader"
mtd: partition "bootloader" extends beyond the end of device "m25p80" -- size truncated to 0x10000
0x000000010000-0x000000010000 : "kernel"
mtd: partition "kernel" is out of reach -- disabled
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
flexcan imx6q-flexcan.0: device registered (reg_base=c0938000, irq=142)
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: Unknown controller version (3). You may experience problems.
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
mmc1: Unknown controller version (3). You may experience problems.
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mmc2: Unknown controller version (3). You may experience problems.
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
VPU initialized
mxc_asrc registered
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx_3stack asoc driver
asoc: mxc-hdmi-soc <-> imx-hdmi-soc-dai.0 mapping ok
ALSA device list:
#0: imx-hdmi-soc
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN4: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
regulator_init_complete: VDDIO: incomplete constraints, leaving on
regulator_init_complete: VDDA: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:05:02 UTC (302)
Waiting for root device /dev/mmcblk1p1...
mmc1: new SDHC card at address aaaa
mmcblk0: mmc1:aaaa SU08G 7.40 GiB
mmcblk0: p1
mmc2: new high speed DDR MMC card at address 0001
mmcblk1: mmc2:0001 SEM08G 7.39 GiB
mmcblk1boot0: mmc2:0001 SEM08G partition 1 2.00 MiB
mmcblk1boot1: mmc2:0001 SEM08G partition 2 2.00 MiB
mmcblk1: p1
mmcblk1boot1: unknown partition table
mmcblk1boot0: unknown partition table
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk1p1): using internal journal
EXT3-fs (mmcblk1p1): recovery complete
EXT3-fs (mmcblk1p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:9.
Freeing init memory: 184K
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
[<80041524>] (unwind_backtrace+0x0/0xf8) from [<80481310>] (panic+0x74/0x18c)
[<80481310>] (panic+0x74/0x18c) from [<80481024>] (init_post+0xa0/0xc4)
[<80481024>] (init_post+0xa0/0xc4) from [<800089bc>] (kernel_init+0xfc/0x128)
[<800089bc>] (kernel_init+0xfc/0x128) from [<8003c8fc>] (kernel_thread_exit+0x0/0x8)
CPU2: stopping
[<80041524>] (unwind_backtrace+0x0/0xf8) from [<800362f8>] (do_IPI+0x10c/0x138)
[<800362f8>] (do_IPI+0x10c/0x138) from [<8003b94c>] (__irq_svc+0x4c/0xc4)
Exception stack(0xbffb5f90 to 0xbffb5fd8)
5f80: 00000021 80617abc bffb5fd8 00000000
5fa0: bffb4000 8064db04 80489408 8061adf4 1000406a 412fc09a 00000000 00000000
5fc0: 00000000 bffb5fd8 8003c958 8003c95c 60000013 ffffffff
[<8003b94c>] (__irq_svc+0x4c/0xc4) from [<8003c95c>] (default_idle+0x24/0x28)
[<8003c95c>] (default_idle+0x24/0x28) from [<8003cb44>] (cpu_idle+0xac/0xe8)
[<8003cb44>] (cpu_idle+0xac/0xe8) from [<1047e3d4>] (0x1047e3d4)
CPU3: stopping
[<80041524>] (unwind_backtrace+0x0/0xf8) from [<800362f8>] (do_IPI+0x10c/0x138)
[<800362f8>] (do_IPI+0x10c/0x138) from [<8003b94c>] (__irq_svc+0x4c/0xc4)
Exception stack(0xbff01f90 to 0xbff01fd8)
1f80: 00000022 80617abc bff01fd8 00000000
1fa0: bff00000 8064db04 80489408 8061adf4 1000406a 412fc09a 00000000 00000000
1fc0: 00000000 bff01fd8 8003c958 8003c95c 60000013 ffffffff
[<8003b94c>] (__irq_svc+0x4c/0xc4) from [<8003c95c>] (default_idle+0x24/0x28)
[<8003c95c>] (default_idle+0x24/0x28) from [<8003cb44>] (cpu_idle+0xac/0xe8)
[<8003cb44>] (cpu_idle+0xac/0xe8) from [<1047e3d4>] (0x1047e3d4)
CPU1: stopping
[<80041524>] (unwind_backtrace+0x0/0xf8) from [<800362f8>] (do_IPI+0x10c/0x138)
[<800362f8>] (do_IPI+0x10c/0x138) from [<8003b94c>] (__irq_svc+0x4c/0xc4)
Exception stack(0xbfd29de0 to 0xbfd29e28)
9de0: 00000000 0000000a 00000001 00000001 00000282 bfd28000 80034c00 bfd28000
9e00: 80608040 806534a0 0bfdc000 00000001 00000000 bfd29e28 80068dcc 80068840
9e20: 20000113 ffffffff
[<8003b94c>] (__irq_svc+0x4c/0xc4) from [<80068840>] (__do_softirq+0x50/0x154)
[<80068840>] (__do_softirq+0x50/0x154) from [<80068dcc>] (irq_exit+0x94/0x9c)
[<80068dcc>] (irq_exit+0x94/0x9c) from [<800362cc>] (do_IPI+0xe0/0x138)
[<800362cc>] (do_IPI+0xe0/0x138) from [<8003b94c>] (__irq_svc+0x4c/0xc4)
Exception stack(0xbfd29e88 to 0xbfd29ed0)
9e80: 8064f060 60000093 80627c7c 80627c7c 8064f06a 8064f099
9ea0: 80627c1c 8064efa8 00000035 8064f06a 00000003 00000001 60000013 bfd29ed0
9ec0: 80064260 800643ac 60000013 ffffffff
[<8003b94c>] (__irq_svc+0x4c/0xc4) from [<800643ac>] (vprintk+0x38c/0x50c)
[<800643ac>] (vprintk+0x38c/0x50c) from [<80481448>] (printk+0x20/0x30)
[<80481448>] (printk+0x20/0x30) from [<8017e72c>] (kjournald+0x88/0x214)
[<8017e72c>] (kjournald+0x88/0x214) from [<8007cb28>] (kthread+0x80/0x88)
[<8007cb28>] (kthread+0x80/0x88) from [<8003c8fc>] (kernel_thread_exit+0x0/0x8)

タグ(2)
0 件の賞賛
返信
1 返信

1,463件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mianbo

one can try to prepare card using attached Linux Guide

Chapter 8 Using a Linux Host to Set Up an SD/MMC Card

and check procedure using Demo Images

http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&appType=license&location=nu... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信