i.MX6 QuadPlus Power Source Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 QuadPlus Power Source Connection

1,457件の閲覧回数
zhirongyang
Contributor I

  From i.MX6 QuadPlus datasheet the VDD_ARM_IN+ADD_ARM23_IN maximum current is 3.73A and VDD_SOC_IN is 3.7A, the NXP QuadPlus reference design(SCH-28615) powered VDD_ARM_IN+ADD_ARM23_IN by PMIC SW2 and VDD_SOC_IN by PMIC SW1, according to the PMIC datahsheet SW2 output capacity is 2.5A and SW1 output capacity is 4.5A, so SW2 canot provide 3.7A current to QuadPlus, I am not sure is it spec error or NXP reference design error? How to use PF0100 F9 or FA OTP to power QuadPlus?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Zhirong

datasheet suggest to use VDD_ARM_IN+ADD_ARM23_IN "CoreMark" = 3370mA

as real life maximum current, while 3.73A 'Power Virus" benchmark test data is given

just for reference. NXP QuadPlus reference design(SCH-28615) works well without

issues related to VDD_ARM_IN max. currents. Also note, that these data are given

for max. junction temperature (105C).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信