iMX6Q : How to work a ONOFF signal pressing a button between 750 ms and 5 seconds ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q : How to work a ONOFF signal pressing a button between 750 ms and 5 seconds ?

974 次查看
koichisakagami
Contributor II

Dear community,
I am checking a ONOFF(Button ) function.

In 10.5 ONOFF (Button) of IMX6DQRM Rev. 3,it said that

"When the chip main power supply is On, a button press between 750 ms and 5
seconds will send an interrupt to the core to request that software bring down the SoC safely."

[Question]

When the pressing a ONOFF button (0.75 ~ 5s) occurs, Is the provided service only IRQ36 ?
Or Is any other service  issued ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 回复

750 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

only IRQ36 is generated, no other service  issued.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复