i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

跳至解决方案
1,729 次查看
m_c
Senior Contributor I

In figure 8-2 USB Boot Flow of IMX6DQRM Rev. 2, it said ARM core will reset if no any activity within 32 seconds when WDOG_ENABLE=1. However, in ERR006282 of IMX6DQCEC Rev. 4. The workaround #2 said, the Watchdog timer begins a 90-second countdown and, if nothing interrupts this process, the part resets.

1. The 32 and 90 seconds. Which one is right?

2. Is this delay time can change or not?

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,480 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,481 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,480 次查看
m_c
Senior Contributor I

Is this timeout value will remain after cold reboot (power off, then power on)?

0 项奖励
回复